Why implement radio frequency identification (RFID) on railroads

Nov 16, 2020

Radio frequency identification (RFID) provides significant benefits for the preventive maintenance and monitoring of railways all over the globe, including asset tracking and reduced costs.

Radio frequency identification (RFID) provides significant benefits for the preventive maintenance and monitoring of railways all over the globe, including asset tracking and reduced costs.
Radio frequency identification (RFID) provides significant benefits for the preventive maintenance and monitoring of railways all over the globe, including asset tracking and reduced costs.

Hundreds of derailments occur on European railroads every year and according to the D-RAIL project, an average derailment has an impact of more than 800,000 EUR. Some of the major reasons for these accidents occurring include wheel, axle, and suspension failures due to wear and tear, as well as incorrect loading. To fix this several hundred million-euro problem, vehicle owners are investing significantly in preventive maintenance and monitoring systems. This requires a complex infrastructure of wayside train monitoring systems (WTMS) such as hot axle box detectors (HABD), axle load checkpoints (ALC), and other devices (ultrasonic sensors, high-resolution cameras, etc.) along the rail tracks.

These systems have already been in place for years. The question now is, why add RFID into that process by tagging each train wagon with on-metal UHF RFID tags and mounting RFID long-range readers at the WTMS? Well, the additional information of the unique RFID tag will enable a link between the critical measured values (detected failure) and the specific vehicle, wheel set, axle, brake, and suspension. Using RFID allows you to know in advance the specific part that requires rework. RFID also provides the following benefits:

  • Reducing maintenance costs
  • Reducing high-cost emergency maintenance
  • Better planning due to real-time information about the vehicle’s condition
  • Higher availability of rail vehicles and better reliability during operation
In addition to improving preventive maintenance, the second reason to implement RFID on railroads is the classical UHF use case: real-time asset tracking.
In addition to improving preventive maintenance, the second reason to implement RFID on railroads is the classical UHF use case: real-time asset tracking.

 

Asset Tracking – Know where your train is

In addition to improving preventive maintenance, the second reason to implement RFID on railroads is the classical UHF use case: real-time asset tracking. This gives all involved parties (vehicle owner, railway undertaking, infrastructure manager, entity in charge of maintenance) the answers to the questions: What? Where? When? And why?

For example, companies in cargo transport can finally have an answer when their customer asks, “Where are my goods/ cargo?” There are also the additional benefits of better planning for vehicle availability and a reduction in unused capacities.

The SICK solution provided for the project is the SICK RFU630 – a UHF RFID read/write device combined with sensors that count the axles.
The SICK solution provided for the project is the SICK RFU630 – a UHF RFID read/write device combined with sensors that count the axles.

 

Why use RFU630 from SICK

During work on a project with Trafikverket, the Swedish transport administration, the team at SICK learned that the following features were significant to the success of the project:

  1. Industrial design
  • Ruggedized housing EN 50125 (shock vibration)
  • Solid electronics compliant with rail norm EN 50121 (EMC)
  • Wide operating temperature range -40°C to +60°C (RFA630)
  • Outdoor IP67 protection class
  1. Fast data processing
  • Read tags > 200km/h
  • Accurate time stamps

The SICK solution provided for the project is the SICK RFU630 – a UHF RFID read/write device combined with sensors that count the axles. This is necessary, not only to assign the tag to the vehicle/wheelset, but also to provide speed, direction of travel, orientation of vehicle, and order of vehicles within the train.

RFID
UHF transponder identification using an RFID read/write device for long sensing ranges
RFU63x

 

Read more

Vision sensors for the detection of rail wear zones on train cars

more

Laser scanners warn about rockfalls and debris avalanches on the tracks of the chinese railroad network

more

The most important questions about RFID easily answered, many application examples and training offers.

Get informed now

Do you have any questions?

Contact our experts