- Home
- About SICK
- SICK "The history"
- Home
- About SICK
- SICK "The history"
SICK's company history
When used in combination with precise optics and intelligent electronics, light can provide the answer to a wide range of issues. This potential was recognized quite some time ago by Dr. E.h. Erwin Sick, who set up his own company back in 1946. In the years that followed, Sick developed his company into a global provider of intelligent sensors and solutions for industrial automation technology.
-
Technology milestones
-
Company development
-
Erwin Sick, company founder
-
-
1950First practice-oriented photoelectric switches based on the autocollimation principle for industrial automation.
-
1951The NT1 close-range scanner:
- A printed mark control device for the packaging industry
- First light curtain for accident prevention on production machines
-
1952
Static accident prevention light curtain with hollow mirror, without mirror wheel.
-
1956
First optical-electronic flue gas monitor based on the autocollimation principle.
-
1959
First rapid optical counter with display and integrated target value definition for quick detection of small objects.
-
1960
First weft winder monitor for very thin knitting thread (autocollimation principle).
-
1962
First optical height scanner for regulating filling levels.
-
1964
First curve control device for guiding a duplicating milling machine according to a construction diagram – the predecessor of today's NC milling machine.
-
1967
Bar-code identification of packing lists, folding boxes, tins, tubes, etc. in the pharmaceutical industry.
-
1970
First luminescence scanner for detecting luminophores in objects.
-
1973
Fiber-optic cable for detecting small objects when space is tight.
-
1975
Introduction of the semiconductor diode for the transmitter beam in photoelectric switches and proximity switches.
First safety grid curtain for controlling protective hoods on eccentric presses.
First color-ring code reader for detecting colored ring codes on ampules.
-
1976
First area scanner with V-shaped, rotating beam and special reflector in safety category 2 for protecting hazardous areas.
-
1978
First in-situ gas measurement device for sulfur dioxide and nitrogen oxide (filter correlator).
First photoelectric switch for detecting the position of a reflector by means of a four-fold reception element. -
1982
First volume flow measuring device based on the ultrasound time-of-flight process.
-
1983
Carbon monoxide measuring device for monitoring emissions in road tunnels.
First use of printed code characters that can be scanned by laser scanners. -
1986
First in-situ diode array spectrometer for sulfur oxide, nitrogen oxide, and ammonia.
-
1989
First distance determination with laser light on the time-of-flight of pulses principle.
-
1991First use of area scanners for site security (e.g., when entering or leaving through lock gates and access points).
-
1993
First area scanner in safety category 3 for protecting hazardous areas.
-
1995
First color sensor.
-
1996
First time-of-flight device for positioning items in high-bay warehouses.
First photoelectric switch with ambient light.
First miniature photoelectric switch with background suppression.
First application of a proximity laser scanner for volume measurement.
First luminescence scanner in the field of automation technology with UV LED.
-
1997
SICK modular advanced recognition technology (SMART) makes it possible to identify even damaged bar codes.
First contrast scanner with dynamic teach-in and high switching frequency. -
1998
First photoelectric proximity sensor which is insensitive to ambient light sources.
-
1999
First photoelectric switch for detecting light sections of a laser line on a 32 x 32 pixel field for determining the shape and position of objects.
First budget photoelectric switch based on time-of-flight technology.
First photoelectric switch with Teflon-coated housing for the electronic and process industry.
First bar code reader with integrated autofocus based on time-of-flight technology.
Smallest fully extrusion-coated magnet sensor
-
2000
Miniature cylinder sensor.
Safety bus system.
-
2001
High-speed 2D code reader.
Teach-in vision sensor.
-
2002
Proximity laser scanner with dynamic protective field switching for automated guided systems.
-
2003
New generation of photoelectric switches: Sensor array with place- and time-triggered measurement of both the object to be detected and especially the environment.
-
2004
3D camera sensors.
-
2004
First high-safety, camera-based safety system for presses.
-
2005
IO-Link: Continuous communication through innovative sensor/actuator interface.
RFID systems make it possible to identify objects without visual contact between reader and object to be identified.
-
2006
Smallest safety laser scanner S300.
-
2007
High-end CCD sensor with integrated illumination.
-
2009
Navigation based on natural landmarks.
-
2010
Color Ranger E: The world's first high-speed 3D camera with high-performance color measurements.
-
2011
EKS/EKM36: New motor feedback system with digital HIPERFACE DSL interface.
MERCEM300Z: Advanced mercury monitoring system with improved sensitivity.
-
2012
GHG-Control: Measuring greenhouse gases instead of calculating them
-
2013
Flexi Loop: The unique, remote integration design of the Flexi Loop allows SICK to meet the demand for cost-saving cascading of safe switches and sensors within a machine. 2013
-
1950
-
1951
-
1952
-
1956
-
1959
-
1960
-
1962
-
1964
-
1967
-
1970
-
1973
-
1975
-
1976
-
1978
-
1982
-
1983
-
1986
-
1989
-
1991
-
1993
-
1995
-
1996
-
1997
-
1998
-
1999
-
2000
-
2001
-
2002
-
2003
-
2004
-
2004
-
2005
-
2006
-
2007
-
2009
-
2010
-
2011
-
2012
-
2013
-
-
1946
The company known today as SICK AG is born:Erwin Sick obtains a license from the American military government in Munich to set up his own engineering firm.1952Presentation of the first marketable accident prevention light curtain at the International Machine Tool Trade Fair in Hanover. The orders that followed led to the initial serial production and the economic breakthrough.1956The company moves to Waldkirch, Germany with its 25 employees.1972The first subsidiary is founded in France.1975The company expands overseas with the founding of a subsidiary in the USA.1988Erwin Sick dies at the age of 79. Gisela Sick takes over from her husband and leads the company as its primary shareholder.1996Erwin Sick GmbH changes its company status to an “Aktiengesellschaft” or joint stock company.1999The first employee shares are issued domestically and abroad.2006SICK celebrates its 60th anniversary.2017SICK now has more than 50 subsidiaries and equity investments as well as numerous agencies around the globe. SICK achieved Group sales of about EUR 1.5 bn. in the 2017 fiscal year with almost 9,000 employees worldwide. -
1909
Erwin Sick was born on November 3 to a train driver in Heilbronn, Germany.1924 - 1928Apprenticeship in the field of optics.1932Start of career at Siemens & Halske, Berlin, as an optical arithmetician; however, the department was closed after six months. He was moved to the laboratory and was given experimental, arithmetic, and constructive tasks, particularly in the area of color film.1934 – 1939Employment – initially as a constructor, later as an engineer – at Siemens, Bosch and Askania working on demanding development projects on color film, cinematics, and astronomical and physical devices.1939 - 1945Laboratory manager at the optical works of A.C. Steinheil & Söhne, Munich.1944Married Gisela Neumann.1945
Became self-employed: In an old barracks in Vaterstetten near Munich, where Erwin Sick lived with his wife, he single-mindedly followed his technological development aims to produce opto-electronic devices. He used the earnings from selling radios he made himself to support his family.1946Founded what was later to become SICK AG on September 26: The apolitical Erwin Sick received a permit from the American military government to practice his profession as an engineer.1949First orders received at the “Achema” fair in Frankfurt after a long hiatus. This was an exhibition meeting for chemical apparatus organized by suppliers to the chemical industry.1951
At the “German Inventor and New Development Trade Fair” in Munich in July, Sick presents the first wooden model he had made of his light curtain and receives a certificate for exceptional creative performance. On October 20, the patent registration for the light curtain invented by Erwin Sick based on the autocollimation principle is the technical breakthrough and forms the basis of an entire range of devices.1956
Relocation of the company – along with its 25 employees – from Oberkirch to Waldkirch into the building of August Faller KG, located at An der Allee 7-9.In October, Sick is granted the patent for a new type of photoelectric retro-reflective sensor that will later become the product with one of the company's strongest sales.1960Founding of the “Institute for Automation” in Munich for developing optoelectronic devices for industrial applications. Sick's main argument for founding the organization in Bavaria's state capital is the shortage of qualified engineers in Waldkirch.1988
Erwin Sick dies on December 3 after suffering a fatal heart attack at the age of 79.