Contact
Feedback

Get to the heart of things with insider information from Smart Motor Sensors

Smart Motor Sensors turn their users into insiders. You could not get any closer to the action! With its Smart Motor Sensors, SICK provides information directly from the center of production. This is information about the status of machines and servomotors that helps to detect malfunctions earlier, solve them more quickly or to avoid them entirely. SICK has once again applied its entire knowledge base to allow customers this insight and to therefore facilitate predictive maintenance procedures. 

 

The Smart Motor Sensors go far beyond the possibilities of conventional motor feedback systems. We have also succeeded in bundling together additional sensor data with the globally established HIPERFACE DSL® one-cable interface for motor feedback systems. This allows real sensor fusion, which is an essential condition for truly smart feedback.

Facts made transparent

The servomotor drives the process. Motor feedback systems supply data for regulating and operating motors and therefore ensure a smooth and efficient process. But motor feedback systems are more than simple data providers. During operation, intelligent sensor technology not only checks parameters such as speed, safe positioning, acceleration, temperature, and the number of revolutions. Predictive maintenance and permanent process condition monitoring are also made possible with additional functions such as the electronic type label, histograms, and user-defined warnings in particular.

This transforms the motor feedback systems from SICK into Smart Motor Sensors.

What is measured?

Speed

Acceleration

Angles

Temperature

Number of revolutions

 

Intelligent one-cable interface – digital evolution with HIPERFACE DSL®

HIPERFACE DSL®

HIPERFACE DSL® from SICK was the first one-cable interface for servomotors on the market. Since then, it has become an established product among manufacturers of motors and drives around the world. This purely digital interface offers a direct connection to the future. The innovative and interference-free HIPERFACE DSL® protocol enables communication using just two wires that are integrated into the motor cable.

Find out more about HIPERFACE DSL®

 

Your benefits – Smart Motor Sensors keep production running

When you combine smart sensor technology with a globally established interface, you get Smart Motor Sensors from SICK.

Smart Motor Sensors are more than just a data source from the center of the drive. Smart Motor Sensors ensure efficient monitoring at any point when something is moving in a process. In many ways, Smart Motor Sensors are therefore the enablers of the future. And the future is here. With HIPERFACE DSL®, Smart Motor Sensors are already enabling condition monitoring and predictive maintenance. Moreover, they transmit reliable speed and position values for intelligent Safe Motion monitoring on the machine. The machine design is more compact thanks to the lack of a second motor connector and a separate encoder cable.

Sensor data

providing information on speed, position, acceleration, temperature, and revolutions

Control

Speed and position information enables safe machine control.

One-cable interface

HIPERFACE DSL® minimizes cabling, as sensor data is transmitted via the motor cable.

 

Industries – performance boost for mechanical engineering

Smart Motor Sensors are at home in all industries. At first glance, this is often not apparent – and yet the intelligent sensors and innovative interfaces from SICK are used in countless servomotors produced by different manufacturers. This provides a wide variety of industries with a crucial boost when it comes to achieving success in production.

Packaging

Robotics

Handling and assembly technology

Semiconductors

Electronics

 

The future starts here

Smart Motor Sensors in Industry 4.0

Smart Motor Sensors meet all the requirements for successful use in Industry 4.0 applications. The most important requirement in this case is HIPERFACE DSL® – the purely digital interface that sends measurement data directly via the servo controller to the cloud or the Ethernet network. On this basis, production processes will be able to network with one another in the future in such a way that they will also work independently.

sHub® - Sensor hub for intelligent servo motors that “say” when maintenance is required

SICK Smart Motor Sensors Sensor Hub Image
  • Additional vibration and temperature data of the sHub® enables high-precision access monitoring – and increases the availability of servo motors
  • The sHub® and EDS/EDM35 make a powerful team; they ensure the integration of relevant safety functions and therefore high-precision and safe servo drives
  • With the digital HIEPRFACE DSL® communication interface, status monitoring of servo motors can be done in real time – with the highest level of safety

sHub® – progress with combined force

The development continues. At SICK, the sensor hub is known as sHub® and is the expansion stage for Smart Motor Sensors. It bundles the data from Smart Motor Sensors and other sensors that are built into the motor. This enables a true sensor fusion. The sHub® “collects” data from Smart Motor Sensors, such as information on safe position and speed, as well as data from other sensor technology, such as temperature, shock, vibrations, and moisture. The sHub® transmits this bundled mass of data via the existing HIPERFACE DSL® data cable synchronously to the drive. Smart Motor Sensors and sHub® are therefore important components as we move towards the Smart Factory in Industry 4.0.

Any questions?

Ask our experts

Sensor solutions for robotics
Robotics image
Sensor solutions for robotics
Robotics image

Working together as equals

Thanks to sensors from SICK, robots perceive more precisely. For all challenges in the field of robotics: Robot Vision, Safe Robotics, End-of-Arm Tooling, and Position Feedback.
Learn more

TOP