Determination of Required Performance Level (PLr)
For each safety function carried out by a safety-related parts of a control system, the required performance level (PLr) must be determined, which often follows these three parameters according to ISO 13849-1:
1. Severity of injury S1:
- Slight (normally reversible injury)
- S2: Serious (normally irreversible injury or death)
2. Frequency and/or exposure to hazard
- F1: Seldom-to-less-often and/or exposure time is short
- F2: Frequent-to-continuous and/or exposure time is long
3. Possibility to avoiding hazard or limiting harm
- P1: Possible under specific conditions
- P2: Scarcely possible
Using the corresponding parameters on the chart below, you can determine the required performance level of a machine. For example, if the severity of injury is slight, you start at S1. You now choose between F1 or F2. If the frequency and/or exposure to hazard is frequent to continuous, you choose F2. If the possibility of avoiding hazard or limiting harm is scarcely possible, we land at P2. This brings us to performance level C, which means we need to operate at this level or higher—so anywhere from PLc to PLe.